Hi There,
I am trying to get an idea of the RAM and Flash use of my program as I have recently bumped into a region overflow issue:
section .bss will not fit in region "m_data"
I am using the MK64FN1M0VLL12 uc with 256KB RAM and 1MB Flash.
I want to statically add an array which is 170*128*2=43520 bytes long.
From what I see in the print size before adding the array only 66560 Bytes are used in RAM so far.
Alas, I get a m_data region overflown by 31732 bytes when I add the array.
Below are code snippets and print size. What am I doing wrong?
Thanks a lot for your help,
S.
-----------------------------------------------
data.h:
extern uint16_t data_current_raw[MEASURES_MAX][BUFLEN];
data.c:
uint16_t data_current_raw[MEASURES_MAX][BUFLEN] = {{0}};
measure.c
#include "data.h"
#DEFINE MEASURES_MAX 170
#DEFINE BUFLEN 128
static uint16_t meas_data_all[MEASURES_MAX][BUFLEN] = {{0}};
(write important data in meas_data_all)
memcpy(data_current_raw, meas_data_all, sizeof(meas_data_all));
Here is the size print before adding data_current_raw:
Invoking: Cross ARM GNU Print Size
arm-none-eabi-size --format=sysv --totals "XXX.elf"
section size addr
.interrupts 1024 0
.flash_config 16 1024
.text 129536 1040
.ARM 8 130576
.init_array 4 130584
.fini_array 4 130588
.interrupts_ram 1024 536805376
.data 1016 536806400
.bss 50172 536807416
.heap 1024 536870912
.stack 1024 536871936
.ARM.attributes 48 0
.debug_info 266651 0
.debug_abbrev 42800 0
.debug_aranges 9744 0
.debug_ranges 10288 0
.debug_macro 243827 0
.debug_line 133816 0
.debug_str 1898995 0
.comment 112 0
.debug_frame 32100 0
.debug_loc 48696 0
.stab 156 0
.stabstr 387 0
Total 2872472
Solved! Go to Solution.
Hi Sylvain,
we can refer K64 reference manual for why SRAM is separated into two parts.
becuase SRAM_L and SRAM_U are accessible by different bus. in some low power mode, for example VLLS2 (Very Low Leakage Stop2), SRAM_L is powered off. A portion of SRAM_U remains powered on.
if your project uses SRAM_L and SRAM_U in same way, I think you can use them together.
for example in ld file, we define m_data as
| m_data | (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00040000 |
| /* m_data_2 | (RW) : ORIGIN = 0x20000000, LENGTH = 0x00030000 */ |
then don't forget allocate related stack and heap to m_data too
after build, there is no error. in map file. we can see meas_data_all and and data_current_raw succesfully allocated.
.bss.meas_data_all
0x1fff00a4 0xaa00 ./source/main.o
.bss.data_current_raw
0x1fffaaa4 0xaa00 ./source/main.o
0x1fffaaa4 data_current_raw
can this help you?
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi Sylvain,
I just copied your code in one of K64 KSDK project, I can reproduce your problem.
you defined
uint16_t data_current_raw[MEASURES_MAX][BUFLEN] = {{0}};
static uint16_t meas_data_all[MEASURES_MAX][BUFLEN] = {{0}};
each of the size is 170*128*2=43520 , so two arrays use 43520*2=87040 bytes code size .
both of these arrays are distributed to .bss section.
in linker file(under C:\Freescale\KSDK_1.3.0\platform\devices\MK64F12\linker\gcc), there are two data areas:
and .bss section is allocated to m_data which total size is 65535 bytes
if we allocate larger memory to .bss. this can solve the problem. here I allocate .bss to m_data2 which has 196608 bytes size, .bss can hold the arrays.
then i built the project again. there is no error.
can you please try the same?
can this help you?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Zhang,
Thanks a lot for the tip, I will have a go and give you an update.
In the meantime can you tell me why the RAM is cut in two part with respectively 25% and 75% of the memory?
What if I want to make use of the full 256KB of RAM?
Thanks,
Sylvain.
Hi Sylvain,
we can refer K64 reference manual for why SRAM is separated into two parts.
becuase SRAM_L and SRAM_U are accessible by different bus. in some low power mode, for example VLLS2 (Very Low Leakage Stop2), SRAM_L is powered off. A portion of SRAM_U remains powered on.
if your project uses SRAM_L and SRAM_U in same way, I think you can use them together.
for example in ld file, we define m_data as
| m_data | (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00040000 |
| /* m_data_2 | (RW) : ORIGIN = 0x20000000, LENGTH = 0x00030000 */ |
then don't forget allocate related stack and heap to m_data too
after build, there is no error. in map file. we can see meas_data_all and and data_current_raw succesfully allocated.
.bss.meas_data_all
0x1fff00a4 0xaa00 ./source/main.o
.bss.data_current_raw
0x1fffaaa4 0xaa00 ./source/main.o
0x1fffaaa4 data_current_raw
can this help you?
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------