ProcessorExpert.ld的m_cfmprotrom这个地址在哪可指定

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ProcessorExpert.ld的m_cfmprotrom这个地址在哪可指定

1,303 Views
andypeng
Contributor I

Kinetis Design Studio Version: 3.2.0,ProcessorExpert.ld的m_cfmprotrom这个地址在哪可指定?比如系统默认

170135_170135.pngpastedImage_1.png

我想变成这样:

   170136_170136.pngpastedImage_2.png

Labels (1)
0 Kudos
Reply
3 Replies

972 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

- You can directly change it on the file of ProcessorExpert.ld , then enable the

"Don't writed generated component modules "by right click the processor component ->

click "code generation"->"Don't writed generated component modules " .

-While this section from 0x0_0400 to 0x0_040F is Flash configuration field , that stores default
protection settings (loaded on reset) and security information that allows the MCU to
restrict access to the flash memory module. We can not change the configuration to other place .


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

972 Views
andypeng
Contributor I

thanks Alice Yang,

   但是按你的提示:

"Don't writed generated component modules "by right click the processor component ->

click "code generation"->"Don't writed generated component modules " .

经过多次测试,发现ProcessorExpert.ld的m_cfmprotrom这个地址我手动改成下面这样:

pastedImage_2.png

再重新 Project->Build Project ,系统有时还会改成下面这样:

pastedImage_1.png

0 Kudos
Reply

972 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andpeng,

Please check the video of the attachment .

Do you right click the processor component ? For example the MK64 .


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply