Hi, I've this problem: can I use the SAME compiler/linker on two different PC ? (of course I mean to have exactly the same compiler/linker/SDK to generate exactly the same binary executable).
Thanks
Hi Salvatore Stefano
KDS and KSDK is a free, open-source software, so it does not have licensing problems and it can be installed in different PC with supported OS. What do you mean by SAME compiler/linker on two different PC ? Do you mean like installing and running KDS on the cloud?
Best Regards
Jorge Alcala
Hi Salvatore Di Stefano,
ARM GCC compiler is included in the KDS installation. It is recommended to remove any previous installation of ARM GCC from your PC before you install KDS.
If you install same version of the KDS on two machines, compiler and linker will be same.
I did not test, if the output is exactly same. May be there are some timestamps, that might be different?
SDK is not included in the KDS, so it is fully under your control, what version will be used.
Regards
Marek