In Kds 3.0 on Linux. Debugging an MK22FN10M (or 512k) part.
in debugger perspective, EmbsysRegister tab. It only shows UARTS 0,1,2 There are SIX Uarts in both of these parts so why are they not displaying and accessable?
I beleive same issue exists for other items like PITs.
Ken
已解决! 转到解答。
Thanks David,
yes that worked... It was set to MK22F51212..so this header is wrong
since this part also has 6 uarts....
In poking around it seems a number of these headers are not complete,
missing both peripheral register defines and int vectors..
Doesn't anybody check this stuff??
Ken
Hi Ken,
Glad to help.
In theory we are checking the stuff....but issues can arise with complex MCU's and software.
What software are you using? KSDK_1.3 or KSDK_v2? Or baremetal?
If using the KSDK drivers, the example projects have #define's in the compiler Preprocessor field that help select processor specific headers.
Example from KSDK_1.3 for frdmk22f project:
DEBUG
CPU_MK22FN512VLH12
FRDM_K22F
FREEDOM
Looking at the KSDK_v2 frdmk22f project has the same Defines.
Regards,
David
David,
using kds 3.0 on Linux, not using sdk. Working on bootloader from code
Alice has sent me.
Using out of the box setup with few changes to make it run, so if you
take the current disti you should see same stuff.
I would also check the linker files, I think they are not quite right
and all of the MKxxx_startup.s files are also missing vectors..
I have the sdk 2.0 for reference and these headers are wrong too, so
seems to be pervasive in older code.
Ken
Hi Kenneth:
I think what you see are the differences between Kinetis parts in the K22-120 MHz family range. Sorry that this caused you confusion so far. I created a document a while ago trying to bring some clarity:
The table does not reflect it, but K22FN1M0 / K22FX512 have 6 UARTs, while K22FN512 has only 3 UARTs.
Regards!
Jorge Gonzalez