PE Component: What does "Legacy" in "Legacy User Components" really indicate?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PE Component: What does "Legacy" in "Legacy User Components" really indicate?

跳至解决方案
769 次查看
ocmonte
Contributor III

Hi,

 

The new KDS 3.0 is finally ready for primetime - *thank you*. C++ out of the box without modification is a huge plus!

 

I do have a question on the PE Component library. The "Legacy" section - should I be using those? I'm interested in using the FSL_USB stack. Are these components being phased out? I've used it for CDC and it seems to work well in three other project using the older CW tools.

 

Cheers,

 

Monte---

标签 (1)
0 项奖励
回复
1 解答
678 次查看
ocmonte
Contributor III

I think I figured it out:

KDS was installed on a machine that currently had some "imported components" on it. Since it did, it named the category "Legacy User Components". I installed KDS on a clean machine and noted that the components I was interested in were not shown or installed. Then I remembered that the other machine had previous installations with imported components. Nothing to worry to about at the moment. These components seem to be functional.

Cheers,

Monte--

在原帖中查看解决方案

0 项奖励
回复
1 回复
679 次查看
ocmonte
Contributor III

I think I figured it out:

KDS was installed on a machine that currently had some "imported components" on it. Since it did, it named the category "Legacy User Components". I installed KDS on a clean machine and noted that the components I was interested in were not shown or installed. Then I remembered that the other machine had previous installations with imported components. Nothing to worry to about at the moment. These components seem to be functional.

Cheers,

Monte--

0 项奖励
回复