OpenOCD doesn't launch on Windows8.1(64bit)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

OpenOCD doesn't launch on Windows8.1(64bit)

跳至解决方案
1,765 次查看
kiyoshimatsuzak
Contributor III

Hi all,

 

I'm developping my software for FRDM-K64F.

I can debug using OpenOCD by KDS3.0 on Windows7(32bit).

But I can't launch OpenOCD by KDS3.0 on Windows8.1(64bit)

 

When I launched OpenOCD, I got pop up message below.

 

79630_79630.pngkds_error.png

 

These images are debug config windows.

79625_79625.pngconfig1.png79626_79626.pngconfig2.png79627_79627.pngconfig3.png79628_79628.pngconfig4.png79629_79629.pngconfig5.png

 

I don't know how should I do.

If you have any advices, please let me know.

 

Regards,

Kiyoshi

标签 (1)
0 项奖励
回复
1 解答
1,515 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kiyoshi,

While your Multilink arrives you could use the P&E OpenSDA interface, please take a look to the step 2 of the following document, it explains how to update the firmware of your board from OpenOCD to the P&E OpenSDA firmware and how to set KDS to debug using it:

https://community.freescale.com/servlet/JiveServlet/download/105199-4-294696/Summary%20of%20FRDM-K64...

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,515 次查看
formator
Contributor I

Hi All

Same error here after fresh install on Windows 8.1 (64bit). I have also try on Windows 10 (64bit) and get same error but don't have any near Win 32bit to test it... Workaround from Carlos works for me but I don't want to use OpenSDAv2/P&E Micro, I would like to use OpenSDAv2.1/mbed CMSIS-DAP.

Did someone found solution on that problem?

thenks

Ervin

0 项奖励
回复
1,515 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kiyoshi,

Have you tried using one of the alternative debug connections P&E Multilink or SEGGER J-Link? Here is a document that explains how to update to this firmware:

Summary of FRDM-K64F open source debug interface

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,515 次查看
kiyoshimatsuzak
Contributor III

Hi Carlos,

Thank you for your advice.

I've ask for an agency of P&E micro.

I'm goint to order multilink.

However, I'd like to develop by my Windows8.1(64bit) laptop, but I don't know where to check.

If you have any idea, please let me know.

Regards,

Kiyoshi

0 项奖励
回复
1,516 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kiyoshi,

While your Multilink arrives you could use the P&E OpenSDA interface, please take a look to the step 2 of the following document, it explains how to update the firmware of your board from OpenOCD to the P&E OpenSDA firmware and how to set KDS to debug using it:

https://community.freescale.com/servlet/JiveServlet/download/105199-4-294696/Summary%20of%20FRDM-K64...

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复
1,515 次查看
kiyoshimatsuzak
Contributor III

Hi, Carlos

I could debug by P&E OpenSDA interface on Windows8.1(64bit).

Thanks a lot!

Kiyoshi

0 项奖励
回复
1,515 次查看
kiyoshimatsuzak
Contributor III

Hi, Carlos

I'm sorry my reply is late.

I got PEMicro's Multilink and I could debug on Windows8.1(64bit) using it.

I'll try your suggestion later.

Thank you so much!

Kiyoshi.

0 项奖励
回复