Open SDA and P&E MultiLink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Open SDA and P&E MultiLink

2,571 Views
vigneshbalaji
Senior Contributor I

Hi,

     Is Open SDA and P&E Multilink are same???

Labels (1)
0 Kudos
Reply
3 Replies

2,223 Views
johnny_pe
Contributor III

Greetings Vignesh,

OpenSDA and P&E Multilinks are not the same.

The OpenSDA platform is a serial and debug adapter that is implemented on many NXP Kinetis development boards. P&E Micro has created firmware applications that can run on some of these OpenSDA boards which make them compatible with P&E's software as well as our control libraries. You can download all of our OpenSDA applications which are targeted to each specific NXP development board here: http://www.pemicro.com/opensda/ http://www.pemicro.com/opensda/

The P&E UNIVERSAL MULTILINK and UNIVERSAL MULTILINK FX are our own line of debug/flash programming interfaces for the Kinetis architecture as well as a variety of other NXP architectures. See more information here: http://www.pemicro.com/universal/

Regards,
Johnny

P&E Microcomputer Systems

0 Kudos
Reply

2,223 Views
BlackNight
NXP Employee
NXP Employee

Hi,

have a read at OpenSDA Serial and Debug Adapter|NXP   and OpenSDAv2 .

OpenSDA is a debug circuit on many NXP boards. It runs a firmware with a bootloader and an application. The application can be written by you, and there are applications from P&E emulating a Multilink, from Segger emulating a J-Link and from ARM/NXP the CMSIS-DAP or mbed application emulating a CMSIS-DAP probe.

I hope this helps,

Erich

0 Kudos
Reply

2,223 Views
DavidS
NXP Employee
NXP Employee

Not really but sort of...

P&E Micro handle the driver firmware for NXP.

When using KDS and KSDK, an example Debug Configuration defaults to supporting the OpenSDA from PEMicro but if you have a USB Multilink you need to make the change in the Debug Configuration to use it as the picture below shows.

ScreenHunter_227 Feb. 11 13.43.gif

Regards,

David

0 Kudos
Reply