NMI disable KE04Z with KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NMI disable KE04Z with KDS

1,991 次查看
george_ch
Contributor II

Good afternoon,

 

I need to disable the NMI from reset.

How to implement in KDS?

 

Thank You

标签 (1)
0 项奖励
回复
5 回复数

1,762 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

if you use processor expert, we can disable NMI pin in CPU component setting.

pastedImage_0.png

if you doesn't use processor expert. we can set SIM_SOPT NMIE bit as 0 to disable it after reset. see below from reference manual

pastedImage_1.png

please note, NMIE is write-once only on each reset. it can only be written after reset.

does this answer your question?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,762 次查看
davidsherman
Senior Contributor I

I'll add that there's another setting under CPU interrupts to disable the NMI interrupt, this also needs to be unchecked in addition to the NMI pin setting.  I had to do this as well.

0 项奖励
回复

1,762 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

yes, this is good. thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,762 次查看
george_ch
Contributor II

Thanks.

I would like to disable NMI from reset.

Your solution disables NMI after reset has occured.

Regards

George

0 项奖励
回复

1,762 次查看
davidsherman
Senior Contributor I

NMI is always enabled at reset, read the Kinetis documentation.  It must be disabled after reset.  For this reason, you have to make sure the pin isn't pulled low at power up or you'll be stuck.

0 项奖励
回复