Looking in to a project that requires graphics and I am trying to use with the K70 board or K60 board.
Which one will have the most tutorials or examples.
Hi Zhang,
Your link https://community.freescale.com/docs/DOC-101586 provides no information
hi dave,
this question was answered in 2014 and this article you mentioned is also old (written in 2014 too). now it changes to version 5. I can't remember what exact it was two years ago.
If I am not wrong it should include a video at that time but now from my side the video can not be showed now.
as a suggestion you could leave your question to the article page, thus if the author sees it he will know.
Jun
Hello Daniel,
please refer thread as below:
https://community.freescale.com/docs/DOC-101586
==========================================
this answer is for you, if it helps, please click on "Correct Answer" button. thanks!
Best Regards,
Zhang Jun
Do you have the files used in that demo on your web sight.
How do I get to the level in which I can do this using the kits.
Date: Fri, 10 Oct 2014 01:19:53 -0700
From: admin@community.freescale.com
To: danieljackmorley@hotmail.com
Subject: Re: - MQX with PEG tutorials
MQX with PEG tutorials
reply from ZhangJennie in Kinetis Design Studio - View the full discussion
Hello Daniel,
please refer thread as below:
https://community.freescale.com/docs/DOC-101586
==========================================
this answer is for you, if it helps, please click on "Correct Answer" button. thanks!
Best Regards,
Zhang Jun
Did your question get answered?
If so, say thanks by clicking Correct Answer in the community thread!
Reply to this message by replying to this email, or go to the message on Freescale Community
Start a new discussion in Kinetis Design Studio by email or at Freescale Community
Following MQX with PEG tutorials in these streams:
Inbox
Hi Daniel.
I suggest you check TWR-K70F120M + TWR-LCD-RGB samples here:
PEG Software Product Line (GUI)|Freescale
| PEG Medical Kiosk: Software offered 'As is', support provided on Freescale Communities only – Example PEG Application for the TWR-K70F120M + TWR-LCD-RGB. Size (K): 2220 Format: exe Rev #: 1.0 Modified: 8/29/2012 | FREESCALE |
| ![]() | |
| PEG MQX HVAC: Software offered 'As is', support provided on Freescale Communities only – Example PEG/MQX Application for the TWR-K70F120M + TWR-LCD-RGB. Size (K): 2868 Format: exe Rev #: 1.0 Modified: 8/29/2012 | FREESCALE |
| ![]() | |
| PEG MQX Web Security: Software offered 'As is', support provided on Freescale Communities only – Example PEG/MQX Application for the TWR-K70F120M + TWR-LCD-RGB. Size (K): 2732 Format: exe Rev #: 1.0 Modified: 8/29/2012 |
Hope this helps!
==========================================
this answer is for you, if it helps, please click on "Correct Answer" button. thanks!
Best Regards,
Zhang Jun