Linker order

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Linker order

跳至解决方案
1,085 次查看
pietrodicastri
Senior Contributor II

Good morning

 

I need a suggestion regarding the linker order. The KDS is defaulting the order of the files in a way that is preventing me

to place the RESET_HANDLER at a fixed predictable address.

I am customizing the bootloader, I need to fix this address, but the routine pattern_fill_gcc is always on top.

How to force the linker order from inside the KDS 3. ???

 

Thank You

 

Pietro

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
983 次查看
BlackNight
NXP Employee
NXP Employee

You can influence the command line passed to the linker here:

pastedImage_0.png

Other than that, you can change/modify the linker file.

Other than that, maybe this helps you:

Putting Code of Files into Special Section with the GNU Linker | MCU on Eclipse

Defining Variables at Absolute Addresses with gcc | MCU on Eclipse

See as well the comments in above articles.

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
984 次查看
BlackNight
NXP Employee
NXP Employee

You can influence the command line passed to the linker here:

pastedImage_0.png

Other than that, you can change/modify the linker file.

Other than that, maybe this helps you:

Putting Code of Files into Special Section with the GNU Linker | MCU on Eclipse

Defining Variables at Absolute Addresses with gcc | MCU on Eclipse

See as well the comments in above articles.

I hope this helps,

Erich

0 项奖励
回复