LPC1768 SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 SDK

6,437 Views
simplethings
Contributor III

Hello everyone,

I am trying to find if LPC1768 is supported by KDS, what I have seen on Welcome to MCUXpresso | MCUXpresso Config Tools , that there is no LPC1768 under listed devices.

I could only find SDK for mbed, and my board already has mbed bootloader installed. However I would like to install one from PE, so that I can use my board with KDS.

Thank you in advance.

9 Replies

5,285 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ivan.

KDS only support most of the Kinetis products, it doesn't support LPC family.

To work with LPC1768 , our recommended IDE is MCUXpresso. You can get it from this url:

MCUXpresso IDE|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,285 Views
simplethings
Contributor III

Thank you ZhangJennie, may I ask one more question about KDS here or should I open a separated thread?

5,285 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ivan.

If you want to ask a new question, I would suggest you open a new thread.

If your question relates with this original question, you could continue ask question here.

Thanks,

Jennie Zhang

0 Kudos
Reply

5,285 Views
simplethings
Contributor III

Well I would like to ask where can I find SDK for LPC1768, I assume I need to download it as I had with KDS.

lpc1768.JPG

Seems like there is no lp1768 on the available board list. I can only find it on "Preinstalled MCUs" but after that I have to choose between multiple wizards, LPCOpen C++, C++ Static ...

0 Kudos
Reply

5,285 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ivan.

There is no MCUXpresso SDK  support LPC1768, so we use LPCOpen library.

Please refer this document of how to create a new LPC project using LPCOpen and MCUXpresso IDE.

https://community.nxp.com/docs/DOC-334959 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,285 Views
simplethings
Contributor III

Thank you Jennie.

On the page you provided I am asked to import the LPCOpen Chip Library for the device used. I couldn't find them in the installation folder of MCUXpresso IDE nor here: LPCOpen Software for LPC17XX|NXP . Where should I get Chip libraries from?

All the best,

Ivan

0 Kudos
Reply

5,285 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ivan.

there is no lpcopen 1768 library. But I know many customer use 1769 as a replacement. you can find it under MCUXpresso install.

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,285 Views
simplethings
Contributor III

Hey Jennie,

thank you one more time. Could you please tell me what bootloader is required for LPC1768 and this IDE. I have mbed bootloader installed, which was preinstalled on the bought board. I do not see any LPC1768 PEMicro bootloader. Also is debugger configuration same as one with KDS?

All the best,

Ivan

0 Kudos
Reply

5,285 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ivan,

I was just back from vacations.

regarding to your question about bootloader, I would suggest you ask LPC engineers here:

https://community.nxp.com/community/lpc 

0 Kudos
Reply