Kinetis design studio version 3.xx is not an option when creating a new project. Why?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis design studio version 3.xx is not an option when creating a new project. Why?

1,379 Views
boliljedahl
Contributor I

@Hello.

 

I am using Kinetis Design Studio version 3.2.0.

 

I have a problem. When I am going to create a new project I don't get the option to create a Kinetis Design Studio project like they do in the blinking LED project on Youtube. I only get the options shown in the attached .PNG file. Why? 

I want to create a KDS 3.xx project.

I am shure it is a check box I have missed. It seems that there are a million checkboxes and I do not have the energy to go through them all. I want to make code to my project not configuring tools.

 

Regards.

 

/Bo

Labels (1)
0 Kudos
Reply
2 Replies

1,295 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bo,

As Erich mentioned, you can select one of the latter two selection .

If you want to make code to your project not configuring tools,

in the "Kinetis SDK" select "None",  and uncheck "Processor Expert":

pastedImage_1.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,295 Views
BlackNight
NXP Employee
NXP Employee

These options all create Kinetis Design Studio projects:

pastedImage_1.png

The first one create SDK projects, while the last one creates both Processor Expert and bare projects for Kinetis Design Studio.

I hope this helps,

Erich

0 Kudos
Reply