Kinetis SDK v2 installation issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis SDK v2 installation issues

跳至解决方案
1,274 次查看
neilporven
Senior Contributor I

Hi everyone,

 

I am trying to get the new FatFs 0.11a or b, so I am trying to update to the new KSDK v2, but I am

experiencing issues while following the install instructions:

 

1. Start the Kinetis Design Studio IDE (section 3.1)

2. Start the Install New Software wizard, from the Help menu.

3. On the Available Software screen, click Add..., to add a new location to Work with.

4. Click Archive, and select to the .zip file provided by KSDK. Then click OK.

5. The Work with box should now be populated, and the list of available software should show Eclipse Update for KSDK in the Processor Expert Software category.

6. Check the checkbox to install Eclipse Update for KSDK.

7. Click Next and follow the on-screen instructions to complete the installation.

 

After doing step 4, step 5 gives me an error

 

Could not find jar:file:/C:/Freescale/SDK_2.0_K64F.zip!/

 

Has anyone experience the same and found a fix?

 

By the way, I have updated the KDS to 3.1.0, so that didn't help.

 

Neil Porven

标签 (1)
0 项奖励
回复
1 解答
819 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Neil:

There is actually not an Eclipse Update in the KSDK v2.0 package. Please have a look at the video Installing KSDK V2.0 New Project Wizard in KDS from the next document:

Using Kinetis Design Studio v3.x with Kinetis SDK v2.0

Regards!
Jorge Gonzalez

在原帖中查看解决方案

1 回复
820 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Neil:

There is actually not an Eclipse Update in the KSDK v2.0 package. Please have a look at the video Installing KSDK V2.0 New Project Wizard in KDS from the next document:

Using Kinetis Design Studio v3.x with Kinetis SDK v2.0

Regards!
Jorge Gonzalez