KSDK... installed but wizard option greyed out?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KSDK... installed but wizard option greyed out?

1,140 次查看
epicedium
Contributor II

So I installed the KSDK 3.0 on OSX following the tutorial here....  Embedded Signal Processing

 

I also built the libraries for a few architectures which compiled fine (I assume this is right for MK20DX256VLK10)

 

93476_93476.pngScreen Shot 2015-10-29 at 22.51.29.png

 

HOWEVER, now when I try to make a project via the wizard, I get... this..

 

Any ideas?

 

93337_93337.pngpastedImage_4.png

标签 (1)
0 项奖励
回复
3 回复数

1,072 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Kris,

ok, thank you for posting this.

In case of any questions about KSDK, please let us know at Kinetis Software Development Kit

Have a great day!

Iva

0 项奖励
回复

1,072 次查看
epicedium
Contributor II

I re-installed and it's working now!

So I think the only issue here is that the installation process seemed to fail with no errors or feedback. The first time I ran the install over lunch, when I got back there was no success/failure notice  (and the KSDK obviously wasn't installed).

Second time, success with a dialogue to tell me so!

0 项奖励
回复

1,072 次查看
epicedium
Contributor II

I did get this message during the KSDK installation:-

Screen Shot 2015-10-29 at 22.58.03.png

I'm re-installing everything now, will update if anything changes

0 项奖励
回复