KSDK... installed but wizard option greyed out?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK... installed but wizard option greyed out?

1,167 Views
epicedium
Contributor II

So I installed the KSDK 3.0 on OSX following the tutorial here....  Embedded Signal Processing

 

I also built the libraries for a few architectures which compiled fine (I assume this is right for MK20DX256VLK10)

 

93476_93476.pngScreen Shot 2015-10-29 at 22.51.29.png

 

HOWEVER, now when I try to make a project via the wizard, I get... this..

 

Any ideas?

 

93337_93337.pngpastedImage_4.png

Labels (1)
0 Kudos
Reply
3 Replies

1,099 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Kris,

ok, thank you for posting this.

In case of any questions about KSDK, please let us know at Kinetis Software Development Kit

Have a great day!

Iva

0 Kudos
Reply

1,099 Views
epicedium
Contributor II

I re-installed and it's working now!

So I think the only issue here is that the installation process seemed to fail with no errors or feedback. The first time I ran the install over lunch, when I got back there was no success/failure notice  (and the KSDK obviously wasn't installed).

Second time, success with a dialogue to tell me so!

0 Kudos
Reply

1,099 Views
epicedium
Contributor II

I did get this message during the KSDK installation:-

Screen Shot 2015-10-29 at 22.58.03.png

I'm re-installing everything now, will update if anything changes

0 Kudos
Reply