KSDK 1.1 w/MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,642件の閲覧回数
w2vy
Contributor V

Is there a list of processors and/or boards that are being added to KSDK 1.1 and MQX for the next release?

 

We are early in the design process and would like to make sure our early designs use a part on the list...

 

After all it should be easy to switch to another (supported) processor later, Right?

 

Tom

ラベル(1)
タグ(2)
1 解決策
1,310件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Tom.


Yes. It will be more easier.


Here is a list supporting devices in KSDK 1.1 and for MQX:

FRDM-K22F

FRDM-K22F-K02*

FRDM-K22F-K02 64*

FRDM-K64F

FRDM-KL03Z - not supported in MQX

FRDM-KL46Z

TWR-K22F120M

TWR-K22F120M-K02*

TWR-K24F120M

TWR-K60D100M

TWR-K64F120M

TWR-KV10Z75M

TWR-KV31F120M

TWR-KV31F120M-KV30*

*These boards do not physically exist, but you can use the associated board to develop code for the subset devices listed. So for instance, if you're interested in the K02 device, use the FRDM-K22F for evaluation but use the K02 libraries provided to write code which will run on the K22F since it is a superset device. as Anthony Huereca mentioned in his post. https://community.freescale.com/thread/336397


I hope it helps.

Iva

元の投稿で解決策を見る

3 返答(返信)
1,311件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Tom.


Yes. It will be more easier.


Here is a list supporting devices in KSDK 1.1 and for MQX:

FRDM-K22F

FRDM-K22F-K02*

FRDM-K22F-K02 64*

FRDM-K64F

FRDM-KL03Z - not supported in MQX

FRDM-KL46Z

TWR-K22F120M

TWR-K22F120M-K02*

TWR-K24F120M

TWR-K60D100M

TWR-K64F120M

TWR-KV10Z75M

TWR-KV31F120M

TWR-KV31F120M-KV30*

*These boards do not physically exist, but you can use the associated board to develop code for the subset devices listed. So for instance, if you're interested in the K02 device, use the FRDM-K22F for evaluation but use the K02 libraries provided to write code which will run on the K22F since it is a superset device. as Anthony Huereca mentioned in his post. https://community.freescale.com/thread/336397


I hope it helps.

Iva

1,310件の閲覧回数
w2vy
Contributor V

Thanks... I guess my post here was kinda off topic...

still getting used to the new forum look and feel...

0 件の賞賛
返信
1,310件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

You are welcome. No problem.

Have a nice day,

Iva

0 件の賞賛
返信