KDS synthiax error but not true

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS synthiax error but not true

ソリューションへジャンプ
2,320件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I have a behaviour with KDS.

The editor is outlining as error an expression, but build time no error is present.

This begun to happen since some time, after the same project has correctly worked for months.

 

Suggestions???

 

Thank You

 

138362_138362.pngkdserr.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,215件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

maybe I don't see it, but I don't see an error in your screen shot?

As a piece of information: Eclipse is using the 'Indexer' for its internal parsing. So it could be that your Indexer database somehow is not correct. See Fixing the Eclipse Index | MCU on Eclipse .

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,216件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

maybe I don't see it, but I don't see an error in your screen shot?

As a piece of information: Eclipse is using the 'Indexer' for its internal parsing. So it could be that your Indexer database somehow is not correct. See Fixing the Eclipse Index | MCU on Eclipse .

I hope this helps,

Erich

0 件の賞賛
返信
2,214件の閲覧回数
pietrodicastri
Senior Contributor II

Yes ,,

Rebuild the index was sufficient,,,

Thank You

0 件の賞賛
返信
2,215件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Pietro,

Can you please provide us a short example reproducing the problem ?

What is the KDS tool version used ?

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信