KDS pre-build scripts and arguments

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS pre-build scripts and arguments

ソリューションへジャンプ
2,263件の閲覧回数
oaf
Contributor IV

Hi,

 

Running KDS-3.0, I use a Python-script to do some work in my project as a pre-build rule.

Command:

    ${SensBin}\CSprojFix.py --src ${ProjHome}\KDS

 

When I make my project I got this output in the Console window:

 

E:\Sensors\Common\bin\KDS\CSprojFix.py --src E:\Sensors\Modules\HDTransceiver\App\KDS

process_begin: CreateProcess(E:\Sensors\Common\bin\KDS\CSprojFix.py, E:\Sensors\Common\bin\KDS\CSprojFix.py --src E:\Sensors\Modules\HDTransceiver\App\KDS, ...) failed.

make (e=193): Error 193

make: [pre-build] Error 193 (ignored)

 

What I don't understand is that the command run by KDS (E:\Sensors\Common\bin\KDS\CSprojFix.py --src E:\Sensors\Modules\HDTransceiver\App\KDS)

works when run from the windows shell, but not from KDS.....

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,029件の閲覧回数
BlackNight
NXP Employee
NXP Employee

If you type a .py command in the Windows shell (aka DOS prompt), it knows about how to call Python with for it.

Try to add

cmd.exe

in front of your command line, so it launches the windows shell/command prompt.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,030件の閲覧回数
BlackNight
NXP Employee
NXP Employee

If you type a .py command in the Windows shell (aka DOS prompt), it knows about how to call Python with for it.

Try to add

cmd.exe

in front of your command line, so it launches the windows shell/command prompt.

I hope this helps,

Erich

0 件の賞賛
返信
2,029件の閲覧回数
oaf
Contributor IV

Hi,

From a quick test, the error-message has disappeared.

But I'm a little bit curious, if the pre-build command is not running through the cmd.exe what is the intended use then? I mean if evry developer in the world using this, must prepend 'cmd.exe' doesn't seem to be logical....

0 件の賞賛
返信