Hello,
If someone is trying to use/install KDS v3.0 on the public beta (4) of OS X El Capitan (10.11), you'll probably have a problem at the workspace selection.
As i found no information about this on the Internet, but solved the problem, here is my solution.
To resolve this problem, I modified the file located here:
"/Applications/KDS_3.0.0.app/Contents/eclipse/kinetis-design-studio.ini" and removed the lines 7 and 8:
To delete:
-showSplash
com.somniumtech.branding.kds
Modified file:
-startup
plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar
--launcher.library
plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.1.200.v20150204-1316
-product
com.somniumtech.branding.kds.ide
--launcher.defaultAction
openFile
-name
Kinetis Design Studio
--launcher.XXMaxPermSize
256m
-vm
features/com.somniumtech.jre.macosx.cocoa.x86_64_1.7.0.76/jre/Contents/Home/lib/jli/libjli.dylib
-vmargs
-Dosgi.requiredJavaVersion=1.7
-Xms256m
-Xmx512m
-XX:PermSize=256m
-XX:MaxPermSize=512m
-XstartOnFirstThread
-Dorg.eclipse.swt.internal.carbon.smallFonts
With that modification, the splash screen is not display and you should be able to choose you workspace and use KDS.