KDS on OS X El Capitan (Beta)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS on OS X El Capitan (Beta)

4,693 Views
valentinpy
Contributor I

Hello,

 

If someone is trying to use/install KDS v3.0 on the public beta (4) of OS X El Capitan (10.11), you'll probably have a problem at the workspace selection.

As i found no information about this on the Internet, but solved the problem, here is my solution.

 

To resolve this problem, I modified the file located here:

"/Applications/KDS_3.0.0.app/Contents/eclipse/kinetis-design-studio.ini" and removed the lines 7 and 8:

 

To delete:

-showSplash

com.somniumtech.branding.kds

 

Modified file:

-startup

plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar

--launcher.library

plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.1.200.v20150204-1316

-product

com.somniumtech.branding.kds.ide

--launcher.defaultAction

openFile

-name

Kinetis Design Studio

--launcher.XXMaxPermSize

256m

-vm

features/com.somniumtech.jre.macosx.cocoa.x86_64_1.7.0.76/jre/Contents/Home/lib/jli/libjli.dylib

-vmargs

-Dosgi.requiredJavaVersion=1.7

-Xms256m

-Xmx512m

-XX:PermSize=256m

-XX:MaxPermSize=512m

-XstartOnFirstThread

-Dorg.eclipse.swt.internal.carbon.smallFonts

 

With that modification, the splash screen is not display and you should be able to choose you workspace and use KDS.

Labels (1)
13 Replies

2,563 Views
mstroven
Contributor III

Thank you so much!

0 Kudos
Reply

2,563 Views
victorperez
Contributor I

Huge Help.  Thank you!

0 Kudos
Reply

2,563 Views
markbereit
Contributor I

Hooray!  Your post rescued me, too!

(Hoping the next update to KDS addresses whatever problem this is, but in the mean time, thank you!)

0 Kudos
Reply

2,563 Views
nestordamiangar
Contributor II

Thanks it worked for me as well

0 Kudos
Reply

2,563 Views
JonathanHess
Contributor III

Yay!

0 Kudos
Reply

2,563 Views
solen
Contributor II

Thanks! Worked for me as well!

0 Kudos
Reply

2,563 Views
allenantony
Contributor II

Worked like a charm!

0 Kudos
Reply

2,563 Views
jrychter
Contributor V

Thanks for posting this!

0 Kudos
Reply

2,563 Views
berrymoist
Contributor I

Thank you very much.

0 Kudos
Reply

2,563 Views
kladu
Contributor II

Works. Thank you!

0 Kudos
Reply

2,563 Views
nirvanauscn
Contributor III

The suggestion works for me with the formal El Capitan released last week.

2,563 Views
vcanuel
Contributor II

Thanks :smileyhappy:

0 Kudos
Reply

2,563 Views
aussiemate
Contributor II

Thank you so much for that comment. 

Was sitting here with a "DeaD" KDS on El Capitan beta 8, which locked up after the splash screen had disappeared, did what you suggested and now works.