KDS limitations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,325件の閲覧回数
joseasensio
Contributor I

Hi everyone!

As I read on documentation, KDS is a complimentary IDE for Kinetis MCU's.

Why complimentary? Isn't it enough to cope the whole software development of a generic application?

 

It has no code-size limitations but, any other kind of limitation?

I know about KDS+SDK support limitations for some parts of Kinetis series processors but, anything else to take in account if these tools will be used with commercial purposes?

 

Thanks a lot.

Jose

ラベル(1)
0 件の賞賛
返信
1 解決策
1,207件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jose,

'complimentary' means 'free of charge'. And yes, you can use it to develop applications for any Freescale Kinetis device. But it is true that for example not every device is supported by the Kinetis SDK.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,208件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jose,

'complimentary' means 'free of charge'. And yes, you can use it to develop applications for any Freescale Kinetis device. But it is true that for example not every device is supported by the Kinetis SDK.

I hope this helps,

Erich

0 件の賞賛
返信
1,207件の閲覧回数
joseasensio
Contributor I

Ups! I was confused about complementary-complimentary differences :smileyhappy:

Thanks for the tip, Erich

Regards

0 件の賞賛
返信
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----