KDS limitations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS limitations

Jump to solution
1,322 Views
joseasensio
Contributor I

Hi everyone!

As I read on documentation, KDS is a complimentary IDE for Kinetis MCU's.

Why complimentary? Isn't it enough to cope the whole software development of a generic application?

 

It has no code-size limitations but, any other kind of limitation?

I know about KDS+SDK support limitations for some parts of Kinetis series processors but, anything else to take in account if these tools will be used with commercial purposes?

 

Thanks a lot.

Jose

Labels (1)
0 Kudos
Reply
1 Solution
1,204 Views
BlackNight
NXP Employee
NXP Employee

Hi Jose,

'complimentary' means 'free of charge'. And yes, you can use it to develop applications for any Freescale Kinetis device. But it is true that for example not every device is supported by the Kinetis SDK.

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
2 Replies
1,205 Views
BlackNight
NXP Employee
NXP Employee

Hi Jose,

'complimentary' means 'free of charge'. And yes, you can use it to develop applications for any Freescale Kinetis device. But it is true that for example not every device is supported by the Kinetis SDK.

I hope this helps,

Erich

0 Kudos
Reply
1,204 Views
joseasensio
Contributor I

Ups! I was confused about complementary-complimentary differences :smileyhappy:

Thanks for the tip, Erich

Regards

0 Kudos
Reply