KDS components library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS components library

1,823 次查看
Ben
Senior Contributor I

Hello

Building a new bare board project:

I can't add components into project, this option is "gray" in RMB menu...

Please help! I am working several days to understand what is wrong, checked all the setup options, but all in vain...

TIA

Benny

5 回复数

1,475 次查看
Ben
Senior Contributor I

Hi Erich

Thank you for the support.

I rechecked my activity, I made a mistake in the new project process, and pressed finish instead of NEXT to check the PE checkbox.

It works now, thanks again.

Benny

0 项奖励
回复

1,475 次查看
BlackNight
NXP Employee
NXP Employee

Hi Benny,

perfect, glad to hear that it works now :-).

Erich

0 项奖励
回复

1,475 次查看
Ben
Senior Contributor I

Thank you Erich, yes, I do mark the PE option in the project, bt it does not work.

Pressing RMB on a component - the 2 upper menu options are gray and you can't select them.

In CW 10.6 I am using it works perfect.

I can't find the reason.

Benny

0 项奖励
回复

1,475 次查看
BlackNight
NXP Employee
NXP Employee

Hi Benny,

can you share at least a screenshot or better the project so I can have a closer look?

Erich

0 项奖励
回复

1,475 次查看
BlackNight
NXP Employee
NXP Employee

Hi Benny,

I assume you are talkign about Processor Expert components? If so, you only can add Processor Expert components to the project, if you have created a Processor Expert project. You can see this if there is a .pe file in the project root folder.

pastedImage_2.png

And then select Processor Expert:

pastedImage_3.png

For SDK v1.3, see Tutorial: Blinky with Kinetis SDK V1.3 and Processor Expert | MCU on Eclipse 

Or: FRDM K64F - blinking an LED using #Kinetis Design Sudio and Processor Expert - YouTube 

I hope this helps,

Erich