I successfully compiled a library in KDS, that was originally written in CodeWarrior.
Now I wanted to create a test-project that uses this library.
I linked the library in the "Paths and Symbols" section of the C/C++ General settings (as a workspace path - the library is still in my workspace).
But when I try to compile the project I get an error that the linker can not find the library:
c:/freescale/kds_1.1.1/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/bin/ld.exe: cannot find -lD:/Freescale_Projects/Freescale_Firmware/MK60_Lib/Debug/MK60.a
The path given here is definitively correct and the file exists.
What can I try?
Regards,
Georg
解決済! 解決策の投稿を見る。
See Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse
especially http://mcuoneclipse.files.wordpress.com/2013/02/gcc-linker-options-for-the-library.png
You need to specify the libarary name with the -I option (without the lib prefix and the .a extension).
See Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse
especially http://mcuoneclipse.files.wordpress.com/2013/02/gcc-linker-options-for-the-library.png
You need to specify the libarary name with the -I option (without the lib prefix and the .a extension).
Thanks a lot, that worked!
But who the hell invents such a strange notation? :smileyconfused:
unfortunately, this is how the GNU linker expect things, and how the GNU linker options are defined.
I believe somehow they thought that this might shorten the command line length. I agree, it is not intuitive at all.
Reference:
https://gcc.gnu.org/onlinedocs/gcc-3.3.6/gcc/Link-Options.html