KDS+arm-none-eabi-gcc 5.4.1: can NOT debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS+arm-none-eabi-gcc 5.4.1: can NOT debug

2,129件の閲覧回数
vaughn
Contributor II

There's no solution to fix KDS: variable optimized out when compile with O2 and LTO option. so i try replace gcc 4.9.1 with higher version 5.4.1.

When using arm-none-eabi-gcc 5.4.1, KDS can not launch debug. so there's maybe a compatibility between KDS and arm-none-eabi-gcc 5.4.1.

KDS launch debug with arm-none-eabi-gcc 5.4.1.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,886件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi,

Did you replace gdb as well? gcc and gdb should be in sync.

I hope this helps,

Erich

0 件の賞賛
返信

1,886件の閲覧回数
vaughn
Contributor II

Thanks Erich, the whole ToolChain is clear to empty and then extract new GCC 5.4 into that folder.

0 件の賞賛
返信