KDS V2.0 ,old and new projects.

cancel
Showing results for 
Search instead for 
Did you mean: 

KDS V2.0 ,old and new projects.

Jump to solution
474 Views
CCandido
Contributor V

Hi,

 

I have problems KDS V2.0, old and new projects.

 

old project:

20065_20065.bmpprj  old  error.bmp

how to re-builder old project,  in new kds?.

 

new project:

 

20078_20078.bmpnew.bmp

 

I use to compiler in PC, XP-SP3

 

thanks.

Carlos

Original Attachment has been moved to: ATPCANMON.zip

Labels (1)
Tags (1)
0 Kudos
1 Solution
165 Views
BlackNight
NXP Employee
NXP Employee

Hi Carlos,

I can build and compile your project without any problems. It seems to be a problem with your PC/environment.

However, Windows XP is not on the supported list of operating systems, so have you tried it on a Windows 7 machine too?

Erich

View solution in original post

0 Kudos
3 Replies
166 Views
BlackNight
NXP Employee
NXP Employee

Hi Carlos,

I can build and compile your project without any problems. It seems to be a problem with your PC/environment.

However, Windows XP is not on the supported list of operating systems, so have you tried it on a Windows 7 machine too?

Erich

View solution in original post

0 Kudos
165 Views
CCandido
Contributor V

Hi Erich,

I tested in Win8 = ok

thanks,

Carlos.

0 Kudos
165 Views
CCandido
Contributor V

Hi Erich,

I use XP-Sp3,

using ( FLASH FILE  to Target ) in ( CW10.5 ) see:

-------------------------

Using restricted address range 0x10000000 to 0x1001FFFF  

Programming file C:\Documents and Settings\Administrador\workspace.kds20\ATPCANMON\Debug\ATPCANMON.elf  

Auto-detection is successful.  

  File is of type Elf Format.  

0 Bytes Programmed, Check Restricted Address Range  

Program Command Succeeded  

-------------------programming ok

KDS2.0: PROGRAMMING

CMD>RE

Initializing.

Target has been RESET and is active.

CMD>CM C:\Freescale\KDS_2.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_1.1.8.201411191655\win32\gdi\P&E\k22fx512m12_pflash_dflash_eeprom_pipeline.arp

Initializing.

Cannot enter background mode. Check connections. 

Error loading programming algorithm - load aborted.

Error occured during Flash programming. not programmer and debug.

PE-ERROR: Error downloading to the device.


new compiling = ok, programmer not.

//----------------------------------------------

project old :

DescriptionResourcePathLocationType
make: *** No rule to make target `all'.  Stop.G6CANCDCC/C++ Problem

thanks

Carlos.

0 Kudos