Hello Ofir Yaish ,
You can have a look at the commone of below thread:
Importing MCU V10.6 projects (sample, using PE and MQX) under KDS
there is a same question with yours , and Pascal Irrle give the solution.
"
As you can see the application is built but the message " Program "gcc" not found in PATH" is always generated.
This error will not impact the project build.
To remove the message you must modify the .cproject file manually as explained in the doc attach and explained in the video too.
"
If still have other error when porting, I strongly recommen you create a new project on KDS, then copy&paste application code into it , I think this is the easiest method for porting .
Hope it helps,
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------