KDS Debug Hardware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS Debug Hardware

1,026 次查看
adamvadala-roth
Contributor I

I'm new to KDS, I am trying to use it to develop firmware for a range of hardware I designed based on the FreeScale MKL05 and MKV10 ARM Cortex M0+ Kinetis chips. For testing and development I have a FRDM-MKL05Z Freedomboard. I'd like to use the FRDM-MKL05Z as a programmer for the target hardware (custom PCBs). I also have a segger J-link debugger probe tool

- Can I use the FRDM-MKL05Z as a debugger for custom PCBs ? If so how do I interface it with KDS all the tutorials only cover other Freedomboards.

- Can I use the Segger J-Link debugger, if so how do I setup the J-Link with Kinetis Design Studio

If you want to know more about the hardware I am working on, I can edit and add more to this post, and I have a project page here: HydroPWNics • Hackaday.io

标签 (1)
0 项奖励
回复
1 回复

895 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please refer below article for  how to Debug External Processors with USBDM and Freedom Board

Debug External Processors with USBDM and Freedom Board | MCU on Eclipse

if i work with MKL05Z16xxx4, i can use below debugger setting to connect board via J-link interface.

pastedImage_1.png


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复