This is happening every time I go to the clock management tab of either a new or existing PE project with sdk 1.3. Its specifically the MCG settings tab that causes the crash within a few seconds of opening it and scrolling down the page without even changing anything on that page.
This also happens across two different computers, a laptop and a desktop.
Screenshot just before opening the tab that causes the issue
and the resulting blue screen, with the error unexpected_kernel_mode_trap
Anyone else have this issue and resolved it? As I said this happens across two different pcs, and it doesn't matter if it's setting up a new project or going to check settings of an exiting one.
This is on Windows 10 version 1703, os build 15063.413 (on both machines)
I've run all the updates for KDS and also windows update but the problem persists.
Kind regards
Ian
已解决! 转到解答。
Hi Ian,
it seems your graphic card/driver is causing this?
I would switch to the no-tabs mode: Switching between ‘tabs’ and ‘no-tabs’ UI in Processor Expert | MCU on Eclipse
Can you give this a try?
I hope this helps,
Erich
Something similar happens on another eclipse based IDE. Going to a specific tab always caused BSOD on Windows 10 Build 1703 but not on build 1607. Microsoft just released an update (KB4022716) that appears to have corrected the problem. I have NOT tried it on KDS 3.2.0 yet but it did correct the issue on another Eclipse product.
Hi Ian,
it seems your graphic card/driver is causing this?
I would switch to the no-tabs mode: Switching between ‘tabs’ and ‘no-tabs’ UI in Processor Expert | MCU on Eclipse
Can you give this a try?
I hope this helps,
Erich