This is happening every time I go to the clock management tab of either a new or existing PE project with sdk 1.3. Its specifically the MCG settings tab that causes the crash within a few seconds of opening it and scrolling down the page without even changing anything on that page.
This also happens across two different computers, a laptop and a desktop.
Screenshot just before opening the tab that causes the issue

and the resulting blue screen, with the error unexpected_kernel_mode_trap

Anyone else have this issue and resolved it? As I said this happens across two different pcs, and it doesn't matter if it's setting up a new project or going to check settings of an exiting one.
This is on Windows 10 version 1703, os build 15063.413 (on both machines)
I've run all the updates for KDS and also windows update but the problem persists.
Kind regards
Ian