KDS 3.0.0 update error - "Unable to connect to repository http://freescale.com/lgfiles/updates/Eclipse/KDS/content.xml"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS 3.0.0 update error - "Unable to connect to repository http://freescale.com/lgfiles/updates/Eclipse/KDS/content.xml"

Jump to solution
1,655 Views
cesar_ramirez
Contributor I

Hello,

 

I installed KDS 3.0.0, and I'm trying to update it using the "Install New Software" option in the "help" menu,

 

then in "Work with:" I select the option "Freescale KDS Update Site - http://freescale.com/igfiles/update/Eclipse/KDS"

 

and appears the next error message:

114194_114194.PNGError KDS update.PNG

 

I appreciate any help, thank's

Labels (1)
0 Kudos
Reply
1 Solution
1,495 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Cecar,

What about your PC system ?  And how about when you choose other options ? For example "All Availabel Sites"

pastedImage_0.png

And where do you install the KDS , i recommend you install it in the default path .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,496 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Cecar,

What about your PC system ?  And how about when you choose other options ? For example "All Availabel Sites"

pastedImage_0.png

And where do you install the KDS , i recommend you install it in the default path .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,495 Views
cesar_ramirez
Contributor I

Hello Alice,

I was at home working with my wireless network and I don't know if it is related but I tried with other network, connecting my laptop with ethernet cable (without wifi), and when I select the "All Availabel Sites" option as you recommended, it worked fine, and shows the list as you. Even the option "Freescale KDS Site Update - http://freescale.com/lgfiles/updates/Eclipse/KDS" now works well and display the following list that I needed:

KDS update worked.PNG

Although I think it isn't necessary, my OS is Windows 7 Home Premium, and installed KDS in the default path (C: \ Freescale \ KDS_3.0.0).

Thank you very much for your help, was very helpful.

César

0 Kudos
Reply
1,495 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Cesar ,

Welcome  !

If you click the correct answer button will be best !:smileyhappy:

Have a great day,
Alice



-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply