KDS 3.0.0 freezes from the start

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS 3.0.0 freezes from the start

968 次查看
taghoter
Contributor II

Hi,

I am a new user both of Mac OS X (currently it is version 10.11.3) and wished to use KDS 3.0.0 (and of course 3.1.0) on Mac. In downloaded the KDS package for OS X and installed it. When starting the program it starts with a splash screen and then ends up asking for a directory to be selected for placing the projects (it seems to be the Eclipse selection prompt), but it completely freezes, it does not allow me to choose or type in anything at all. I would rather like to test something to get it solved, but I do not know how to proceed.

If you suggest me any hint I would be very grateful.

Greetings,

Tomás.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

754 次查看
BlackNight
NXP Employee
NXP Employee

Hi Tomas,

there is a known problem with El Capitan, see KDS on OS X El Capitan (Beta)

I hope this helps,

Erich

0 项奖励
回复

754 次查看
taghoter
Contributor II

Hi, Erich,

Thanks a lot for your hint. It has worked pretty fine.

Greetings.

0 项奖励
回复