KDS 3.0.0 freezes from the start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS 3.0.0 freezes from the start

917 Views
taghoter
Contributor II

Hi,

I am a new user both of Mac OS X (currently it is version 10.11.3) and wished to use KDS 3.0.0 (and of course 3.1.0) on Mac. In downloaded the KDS package for OS X and installed it. When starting the program it starts with a splash screen and then ends up asking for a directory to be selected for placing the projects (it seems to be the Eclipse selection prompt), but it completely freezes, it does not allow me to choose or type in anything at all. I would rather like to test something to get it solved, but I do not know how to proceed.

If you suggest me any hint I would be very grateful.

Greetings,

Tomás.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

703 Views
BlackNight
NXP Employee
NXP Employee

Hi Tomas,

there is a known problem with El Capitan, see KDS on OS X El Capitan (Beta)

I hope this helps,

Erich

0 Kudos
Reply

703 Views
taghoter
Contributor II

Hi, Erich,

Thanks a lot for your hint. It has worked pretty fine.

Greetings.

0 Kudos
Reply