K64 suport in MCUXpresso-IDE??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 suport in MCUXpresso-IDE??

2,272件の閲覧回数
davenadler
Senior Contributor I

NXP has announced MCUXpresso replaces KDS.
However, this web page shows support only for K2x (under Supported Devices):
http://www.nxp.com/products/software-and-tools/run-time-software/mcuxpresso-software-and-tools/mcuxp... 

When will MCUXpresso support K64F?

タグ(3)
0 件の賞賛
返信
4 返答(返信)

1,509件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Dave,

two usefull links: 

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信

1,509件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Dave,

it does support the K64F, and in fact supports all the devices supported by the SDK V2.x.

The list you can see if you go to Welcome to MCUXpresso | MCUXpresso Config Tools 

pastedImage_2.png

Create the SDK for your device of choice, and then have it added to the IDE ( Video Link : 7489 ).

I hope this helps,

Erich

0 件の賞賛
返信

1,509件の閲覧回数
davenadler
Senior Contributor I

So the list of supported devices on the above web page is incomplete?

0 件の賞賛
返信

1,509件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

you mean this page of devices?

http://www.nxp.com/products/software-and-tools/run-time-software/mcuxpresso-software-and-tools/mcuxp... 

MCUXpresso IDE is derived from LPCXpresso. LPC devices are supported natively, but there is no Kinetis device preinstalled in MCUXpresso.

However all the Kinetis SDK2.x supported device can be installed to MCUXpresso. Thus MCUXpresso can work with Kinetis with SDK2.x.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信