I have a customer that has designed with the Freescale MK10DX256VLH7 processor in their product. They used Kinetis design studio v1.1.1 to create a project that sets up drivers for the set of resources we use on that processor. In that version of KDS it was possible to specify our own vector handlers for SVC_Handler, PendSVC_Handler and SysTick_Handler. We are also using a Freescale MK02FN64V part in another component of our product. That processor is only supported through KDS 2.0.0. I installed and used this version of KDS to create a project to drive the resources we are using on the MK02FN64V processor. The problem is that I cannot find any way through this version of KDS to specify my own vector handlers. This is very important to us. Does 2.0.0 have the ability to specify vector handling? And if so...how can I do it? Thank you.
Hello Steve Mitropoulos:
Vector handler names are specified in the file called startup_MK02F12810.S. You simply need to declare your own ISR functions. Please check the next discussions in community about this:
interrupt without processor expert in KDS
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------