Is it possible to use Processor Expert (in KDS3.2) for setting up ADC HW Average (KL43z)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to use Processor Expert (in KDS3.2) for setting up ADC HW Average (KL43z)?

1,400 Views
agor53
Contributor II

Hi,

I use Processor Expert in KDS3.2 with SDK1.3 for FRDM KL43z.

I can't find HW average settings.

Thanks in advance,

Andrey

Labels (1)
3 Replies

1,254 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andrey,

You can use the  component of "Init_ADC" :

pastedImage_1.png

Hope it helps

ALice

1,254 Views
agor53
Contributor II

Hi, Alice

Thank you very much, I was blind to see this component.

Andrey

0 Kudos
Reply

1,254 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andrey,

Welcome !


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply