Installing KDS 3.0 in Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Installing KDS 3.0 in Linux

2,165 次查看
karfes
Contributor II

I donwloaded the binary and tried to install several times, it spits out an error about unwanted newline and something about "Arch". Its a 64 bit binary and I have Ubuntu 14.04 64-bit. Whats up? Anyone successful?

标签 (1)
0 项奖励
回复
5 回复数

1,917 次查看
superguys
Contributor I

I had to add .deb to the file name. Then I could use the package manager to install it.

0 项奖励
回复

1,917 次查看
karfes
Contributor II

Yeah, I figured that out, they named the file .bin by default, dont know why. I thought it was an binary file to be executed by sh or bash.

0 项奖励
回复

1,917 次查看
superguys
Contributor I

That bit me as well. I am glad you figured it out.

0 项奖励
回复

1,917 次查看
karfes
Contributor II

How to add Kinetis SDK? please.  Kinetis design studio 3.0 in Linux

0 项奖励
回复

1,917 次查看
BlackNight
NXP Employee
NXP Employee

I'm not sure why the extension from the file download is currently .bin. I have requested to change/fix the extension to .deb.

Thanks to David and Isaac for reporting it (along with the solution).

0 项奖励
回复
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----