Importing CW project to KDS v3.2.0 - Help Needed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Importing CW project to KDS v3.2.0 - Help Needed

824 Views
Deejay
Contributor III

Hi,

I'm trying to import a project originally created in CW10.6 into KDS v3.2.0 but no success. I keep getting the following warning messages.

163845_163845.pngpastedImage_1.png

 

 

Under the project properties for C/C++ Build, i have the following warning and the tool settings empty.

Could someone let me know how i can fix this please?

 

163846_163846.pngpastedImage_2.png

 

Thank you.

DJ

Labels (1)
0 Kudos
5 Replies

619 Views
sivaveluppillai
Contributor III

As I said the issue is not that simple!

There are many headers that are specific to CW that is not compatible to this new KDS environment.

I am getting errors even importing the examples - could we import the examples direct?

Also copy the .project file to the project method is not working in KDS?   

0 Kudos

619 Views
mjbcswitzerland
Specialist V

Hi

If you need a fast and guaranteed solution for commerical work you can contact http://www.utasker.com/support.html where CW to KDS project conversions can be made for you for a small fee.

Regards

Mark
Kinetis for professionals: http://www.utasker.com/kinetis.html

0 Kudos

619 Views
MarekTrmac
NXP Employee
NXP Employee

Hi,

I'd recommend to create new project in KDS using New Project Wizard and then add sources you want to build. That's probably easiest way how to do it.

Regards

Marek

0 Kudos

619 Views
mjbcswitzerland
Specialist V

Hi Devan


CW and KDS are not compatible - there may be some method of modifying the projects of one to become compatible with the other IDE but is is probably easiest to just create a new project in KDS.

The uTasker projet maintains two project sets so that both KDS and CW can be used interchangeably - see http://www.utasker.com/kinetis/compilers.html#KDS
which works fine although may not be the simplest solution....


Regards

Mark

Kinetis for professionals: http://http://www.utasker.com/kinetis.html

0 Kudos

619 Views
sivaveluppillai
Contributor III

This means KDS doesn't s provide a good migration path for CW projects.

How do you handle the headers that are specific to CW that is not compatible to this new KDS environment?

0 Kudos