Hi,
I'm trying to import a project originally created in CW10.6 into KDS v3.2.0 but no success. I keep getting the following warning messages.
Under the project properties for C/C++ Build, i have the following warning and the tool settings empty.
Could someone let me know how i can fix this please?
Thank you.
DJ
As I said the issue is not that simple!
There are many headers that are specific to CW that is not compatible to this new KDS environment.
I am getting errors even importing the examples - could we import the examples direct?
Also copy the .project file to the project method is not working in KDS?
Hi
If you need a fast and guaranteed solution for commerical work you can contact http://www.utasker.com/support.html where CW to KDS project conversions can be made for you for a small fee.
Regards
Mark
Kinetis for professionals: http://www.utasker.com/kinetis.html
Hi Devan
CW and KDS are not compatible - there may be some method of modifying the projects of one to become compatible with the other IDE but is is probably easiest to just create a new project in KDS.
The uTasker projet maintains two project sets so that both KDS and CW can be used interchangeably - see http://www.utasker.com/kinetis/compilers.html#KDS
which works fine although may not be the simplest solution....
Regards
Mark
Kinetis for professionals: http://http://www.utasker.com/kinetis.html