In my Kinetis Design Studio IDE (2.0.0), I am trying to start a new project (Kinetis Design Studio Project), unfortunately the FRDM-KL03Z doesn't appear
as a selection? I do see the FRDM-K64F, which I also have?
I downloaded the following : KSDK_1.0.0-KL03Z
I am not sure where to go from here, I need help?
Thanks,
Neil
Hello Neil,
please, use the newest KSDK 1.1. and it appears with KL03Z.
Please install it according to your platform
Software Development Kit for Kinetis MCUs|Freescale
If you use KSDK 1.0. is needed special standalone patch.
I hope it helps,
Best Regards,
Iva
Not sure why they only have a couple of the boards, but I never had a problem making a project to target the processor and not the board. For the FRDM-KE06 I just targeted the KE06Z processor on the board and it worked fine.
Hello Neil Porven:
All new support in KDS comes with the KSDK releases but an Eclipse Update needs to be installed first. I recommend you to download the latest version of KSDK (v1.1.0) and install the support following instructions in the next document:
How to install Kinetis SDK 1.1.0 support in KDS 2.0.0
David Sherman:
Only the boards supported by the KSDK platform are listed under "Boards".
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------