How to use UART_2 on K22F Board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use UART_2 on K22F Board?

1,775件の閲覧回数
randalford
Contributor II

I wish to connect a serial device (WIFI Module) to the K22F board. If I am reading the schematic correctly, my best option is to use UART_2 on the J3 port. I cannot find any documentation or examples that do not use "mbed.h" and that file is not available. I am using Kinetis Design Studio Version: 3.2.0. I want to be able to still use the Debug UART as that is working properly.

 

What are my options for connecting an external module? Is there a way to add "mbed.h" to KDS? Links to applicable documentation is appreciated.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,587件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Randal,

Do your meaning the FRDM-K22F board  or TWR-K22 board?

Yes, you can use the UART2.

And about the mbed.h ,do you want to use mebd or do not want ? And on KDS, we can

not sue it .

If i misunderstand you , please tell me .

BR

Alice

0 件の賞賛
返信

1,587件の閲覧回数
randalford
Contributor II

FRDM-K22F board.

I am trying Kinetis Design Studio Version: 3.2.0 for now, but can use something different if I have to.

I want to find a development system that provides ALL peripheral drivers for the MK22fN512VLH2.

I found some examples that used mbed.h. I do not know anything about it.

0 件の賞賛
返信

1,587件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Randal,

Ok, on KDS v3.2, you can install the SDK_2.0_FRDM-K22F , it include all of the drives and some demo code :

pastedImage_0.png

About how to download and install it , there is a DOC guide for step by step :

Using Kinetis Design Studio v3.x with Kinetis SDK v2.0

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信