How to program MKE04Z8VTG4?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to program MKE04Z8VTG4?

1,323 次查看
sergiostarkloff
Contributor I

we made a hardware with this

someone told me that I will be able to program with ST-Link, but.... no

which hardware I need?

标记 (1)
0 项奖励
回复
1 回复

1,125 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

There are several IDE and Probes we can use for MKE04.

For example NXP has these IDEs support it:

Kinetis® Design Studio Integrated Development Environment (IDE)

CodeWarrior® for MCUs (Eclipse IDE) - ColdFire®, 56800/E DSC, Kinetis®, Qorivva® 56xx, RS08/S08, S12...

PE emulators are widely used for this chip

Universal Multilink Development Interface

Universal Multilink FX High-Speed Development Interface

Seger JLink is also good for debuging and programming.

For more, please check this url

Arm Cortex-M0+|Kinetis KE04 48 MHz 32-bit 5V MCUs|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复