Hello,
I'm new with FreeScale but I managed to setup KDS and rebuild the 'hello_world' application for KL25Z.
Now I want to run it on a board.
But the target I created is in .elf format.
To be able to run it on the KL25Z I must convert it to BS. (.Sxx or .bin)
According to information I found this can be achieved with the 'elftobs' converter.
But I cannot find this tool on NXP of any other site. I found github where it can be downloaded and build.
Can do that, but I like to use the original application first.
If someone knows where to find elftobs (or elftobin) I like to hear.
Thanks,
Jan
Solved! Go to Solution.
Hi,
elftobs is included in NXP_Kinetis_Bootloader_2_0_0 package.
download link:
folder: ..\Freescale\NXP_Kinetis_Bootloader_2_0_0\bin\Tools\elftosb
this tool is for generating "Secure Binary" file. the "key file" is needed for using elftobs tool.
if you only need generate a project bin or srec file, KDS itself can do it well. elftobs is not needed. I just made a video of how the KDS generates bin and srec files. Hope this helps!
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks, both of you.
The answer of Jennie Zhang best reflected my question and the video was very welcome either.
But from Erich I learned that there are other useful tools to explore.
Now I can make the next step.
Jan
Hi Jan,
KDS includes the 'objcopy' utility which can directly create s19, binary or intel hex files (see https://mcuoneclipse.com/2014/04/20/binary-files-for-the-mbed-bootloader-with-eclipse-and-gnu-arm-ec... ). For any other advanced binary file manipulation, I recommend the Srecord utility (see https://mcuoneclipse.com/2015/04/26/crc-checksum-generation-with-srecord-tools-for-gnu-and-eclipse/ ).
I hope this helps,
Erich
Hi,
elftobs is included in NXP_Kinetis_Bootloader_2_0_0 package.
download link:
folder: ..\Freescale\NXP_Kinetis_Bootloader_2_0_0\bin\Tools\elftosb
this tool is for generating "Secure Binary" file. the "key file" is needed for using elftobs tool.
if you only need generate a project bin or srec file, KDS itself can do it well. elftobs is not needed. I just made a video of how the KDS generates bin and srec files. Hope this helps!
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Nice video! I have a newer version of KDS (ver. 3.2) - and I don't have a toolchain tab. There's a toolchain editor - but I didn't know what do with it.
I'd like to generate an sreg file for the MSD Flash Programmer on my FRDM-KE04Z board. I'm not clear if KDS can still do this on its own or if I need to install something.
Okay, KDS 3.2 has a toolchain tab. I mistakenly had a file highlighted instead of the project name in the project tree highlighted - so when I right clicked and selected properties I got the dialog shown above in the screen capture. Anyway, once I highlighted the project name at the top of the tree I was able to access the toolchain and adjust the settings as shown in the video. Thanks!