Hi, I have to compute some values like current and resistance by software. I mean, I set a particular voltage from 0V to 3.3V ( so from 0 to 65534, for 16 bit) by software on a Digital to Analog Converter, then I want to compute the current, so I define the resistance (for example for 1 ohm resistance, I will write R= 19858, considering 16 bit, i Don't know if it is right) and then I compute the current I= voltage/R; Now, first of all, I don't know if it is possible to compute the current in this way, please, let me know how can I do. The second problem is that I want to verify this result, I mean, i want to veify if the current is right and I want to see the value of I (the current), on arduino I used the serial port and I wrote printf ("current", I); and i could see the result, is there a way to see the results on KDS? Thank you
已解决! 转到解答。
Hi,
i think your solution of calculating current is OK.
regarding how to see result with KDS, i suggest you use printf. here is an article for this topic,
How to use printf() to print string to Console and UART in KDS2.0
can this help you?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello
Your calculation is a bit confusing (for me)
Here ist my way to solve that problem (if you can use float-values):
float R = 1; // [Ohm]
int16_t U_raw = acd_get_result(); // replace with your function
float U = (float)U_raw * ( 3.3 / 2^16 ); // [Volt] (or replace (3.3/2^16) with 0.00005)
float I = U / R; // [Ampere]
Peter
Hi,
i think your solution of calculating current is OK.
regarding how to see result with KDS, i suggest you use printf. here is an article for this topic,
How to use printf() to print string to Console and UART in KDS2.0
can this help you?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------