Hi Sir :
There are many Kinetis device can not be found in KDS3.0 Embsys register viewer . For example , KE , KM , KV3 , KV4 .... series .
Is there any update to add those device in register viewer ?
Thanks .
David
解決済! 解決策の投稿を見る。
Hi,
please make use you have all KDS updates installed.
if still can't find the missing device,
please unzip attached package and copy the content into your KDS embsysregview install folder
C:\Freescale\KDS_3.0.0\eclipse\plugins\org.eclipse.cdt.embsysregview.data_0.2.4.freescale\data\SVD(CMSIS)\Freescale
there is 107 devices included, KE , KM , KV3 , KV4 .... series are also included.
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Zhang Jun and Erich :
Much thanks for your kindly support .
I found the issue why my KDS3.0 miss so many Freescale device .
There are two embsysregview in my KDS folder , one is Ver 0.2.4 another is 0.2.5.r180 .
I checked "Freescale " folder in those embsysregview folder .
Ver0.2.4 support a lot of Freescale Kinetis device .
Ver 0.2.5.r180 only support a little standard parts .
However , Ver 0.2.5.r180 embsysregview is engaged in my KDS3.0 , so many Kinetis device are missed .
Now I copy Jun's attach file to 0.2.5.r180 folder , and it works .
Thanks again .
David
The EmbSysRegView uses normal SVD files (with .xml extension).
These are the ones which come with KDS v3.0.0:
The files are inside
C:\Freescale\KDS_3.0.0\eclipse\plugins\org.eclipse.cdt.embsysregview.data_0.2.4.freescale\data\SVD(CMSIS)\Freescale
I hope this helps,
Erich
Hi,
please make use you have all KDS updates installed.
if still can't find the missing device,
please unzip attached package and copy the content into your KDS embsysregview install folder
C:\Freescale\KDS_3.0.0\eclipse\plugins\org.eclipse.cdt.embsysregview.data_0.2.4.freescale\data\SVD(CMSIS)\Freescale
there is 107 devices included, KE , KM , KV3 , KV4 .... series are also included.
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------