How to add a board to Kinetis Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add a board to Kinetis Design Studio

ソリューションへジャンプ
2,669件の閲覧回数
eduardoumana
Contributor III

When I create a new "Kinetis Design Studio Project," only the K64F board is listed. How can I add the K22F board, which I am using, to Kinetis Design Studio?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,896件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Eduardo,

Boards and new devices are added to KDS with the Kinetis SDK.

So download the K22F Kinetis SDK (SDK V1.0.0) from www.freescale.com/ksdk, then install it.

Use in KDS the menu Help > Install New software and use the zip file from

C:\Freescale\KSDK_1.0.0\tools\eclipse_update

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,896件の閲覧回数
jverive
Contributor III

Eduardo,

Also remember to follow instructions for building the platform driver library (see the appropriate section in the Kinetis SDK K22 User's Guide). You may already have been aware of this, but it was a huge source of frustration to me getting started with my K22F board.

Jeff

0 件の賞賛
返信
1,897件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Eduardo,

Boards and new devices are added to KDS with the Kinetis SDK.

So download the K22F Kinetis SDK (SDK V1.0.0) from www.freescale.com/ksdk, then install it.

Use in KDS the menu Help > Install New software and use the zip file from

C:\Freescale\KSDK_1.0.0\tools\eclipse_update

I hope this helps,

Erich

0 件の賞賛
返信
1,896件の閲覧回数
carloshass
Contributor II

Erich,

The TRK-KEA Boards are not supported by KDS?

0 件の賞賛
返信