How I can program FRDM-KL28Z with KDS and PEx?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How I can program FRDM-KL28Z with KDS and PEx?

ソリューションへジャンプ
1,241件の閲覧回数
OmarIsaiPinales
Contributor II

Hello, I tried to create a new Processor Expert project in Kinetis Design Studio for FRDM-KL28Z, but I can't find the board or the processor, are there someone who knows how to do this? I will be very grateful.

ラベル(1)
タグ(2)
1 解決策
1,067件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

KDS3.2 itself doesn't support KL28 yet. user who need work with KL28 please use KDS3.2+KSDK2.0 instead.

here is to download KL28Z SDK2.0 package

Welcome to Kinetis Expert | Kinetis Expert

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,067件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Omar,

KDS 3.2 does support this device. Support for it is delivered with the SDK package generator, so you have to build first the SDK you want on Welcome to Kinetis Expert | Kinetis Expert , then import and use it with KDS. See https://mcuoneclipse.com/2016/01/29/first-nxp-kinetis-sdk-release-sdk-v2-0-with-on-demand-package-bu... .

I hope this helps,

Erich

1,068件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

KDS3.2 itself doesn't support KL28 yet. user who need work with KL28 please use KDS3.2+KSDK2.0 instead.

here is to download KL28Z SDK2.0 package

Welcome to Kinetis Expert | Kinetis Expert

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------