Frequency output change on KL25Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Frequency output change on KL25Z

ソリューションへジャンプ
1,594件の閲覧回数
tommyb90
Contributor III

Hi to everyone,

Using an FRDM-KL25Z dev. board I have to give a frequency output and update its period every once in a while.

 

I tried using the TimerOut component on KDS3.0, but it seems that I am not able to change the period of the timer (I wanted to enable the SetPeriodUS method, but it was not possible).

 

I also tried using the PWM component, but again I am not able to set the period of the output signal.

 

Is there another way to generate this kind of output?

 

Thanks in advance,

        Tommaso

ラベル(1)
0 件の賞賛
返信
1 解決策
1,379件の閲覧回数
tommyb90
Contributor III

Thanks for your reply,

I ended up fixing the issue by giving the PPG component an interval in which the period could be valid (set interval instead of fixed value inside the period setting window). This enabled the SetPeriodUS Method, but limited my choice in the frequency.

Thanks for everything

        Tommaso

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,379件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tommas,

Does this can help you ?

https://community.nxp.com/message/346460 

BR

Alice

0 件の賞賛
返信
1,380件の閲覧回数
tommyb90
Contributor III

Thanks for your reply,

I ended up fixing the issue by giving the PPG component an interval in which the period could be valid (set interval instead of fixed value inside the period setting window). This enabled the SetPeriodUS Method, but limited my choice in the frequency.

Thanks for everything

        Tommaso

0 件の賞賛
返信