Mine is working. when i try to transmit K i get an error. because anyone ack the data and i am able to view
at the oscilloscope data being transmitted.
what i have done was. delete all files in the board folder and substitute them for the files in a FRDM sample.
*********FlexCAN : SCI2CAN demo *********
Message format: Standard (11 bit id)
Message buffer 8 used for Rx.
Message buffer 9 used for Tx.
OSJTAG Port used for Serial Console.
Interrupt Mode: Enabled
Operation Mode: TX and RX --> Normal
*****************************************
Please select local node as A or B:
Node:AA
k
Transmit send configuration failed. result: 0x5
FlexCAN demo failed!!
I would like to know what 0x5 error means i have searched but in the doc. they only say 0 ok not 0 error.