Flashing KBOOT and Initial App

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing KBOOT and Initial App

Jump to solution
1,610 Views
alex323qp
Contributor III

Hi everyone, I'm trying to flash a custom bootloader based on the KBOOT 1.2 and also an initial app to my target KL25Z64 through KDS, using the PEMicro Universal Multilink FX. I'm first flashing the base app (with the right start location) and then the bootloader (.elf files), but it looks like on every flashing the previous binary gets replaced, is there any "right" procedure I'm not following?

 

p.s I also tried unchecking the "Mass erase on connect" checkbox without success.

107695_107695.pngpastedImage_0.png

 

Thanks in advance,

 

Alex.

Labels (1)
0 Kudos
Reply
1 Solution
1,212 Views
alex323qp
Contributor III

The answer was right under my nose:

For those that may have the same question, you can "Preserve" Memory ranges from the "Advanced Options" button.

More information here: preserved memory range problem in KDS 3.0

Cheers,

Alex.

View solution in original post

0 Kudos
Reply
1 Reply
1,213 Views
alex323qp
Contributor III

The answer was right under my nose:

For those that may have the same question, you can "Preserve" Memory ranges from the "Advanced Options" button.

More information here: preserved memory range problem in KDS 3.0

Cheers,

Alex.

0 Kudos
Reply